Other Parts Discussed in Thread: CCSTUDIO
Hi,
I am new to CCS V5 (I used to use CCS V3.3). I have just installed CCS V5 (CCS5.1.1.00031_win32) and was trying to build a simple test project (under Windows XP).
How can I add a new Emulator type in CCS V5? I have installed a Softronics XDS 510 PCI jtag and a SEED USB XDS560. both run under CCS 3.3. For the SEED, I installed the CCS V4-setup.exe. Both devices are visible as 'working' in the Windows XP device manager, the softronics XDS510 is recognized as Texas Instruments XDS560...:

In the old CCS 3.3 Setup, the XDS510 emulator shows up like this - I can connect to DM648, C6204 and C6414:


In CCS V5.1, neither of the 2 emulators shows up in the list of emulators that is available in the 'Project Properties - General - Connection'. I tried to select different options, but get always the 'Unable to communicate with the emulator' error dialog.

What is the standard procedure to extend CCS V5 by emulator drivers?
Any experiences with the SEED XDS560 USB or the Softronics XDS510 PCI Jtag under CCS V5?
bye,
Thomas