This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using C6713 DSK(CCS v3.1) with CCS v3.3



   when I try to build model in Simulink for the C6713DSK board it gives the error below.

Error using ==> LinkCCS at 28

Error while connecting to Code Composer Studio(tm):

Error using ==> cu_compareAndWarnCCSVersions at 53

This version of the Embedded IDE Link CC does not support your
version of Code Composer Studio(TM) IDE.
The Code Composer Studio(TM) version supported in this release is 3.3.
Refer to the Embedded IDE Link CC data sheet
for more information on product requirements.
CCS v3.1 came with the DSK. I have got the CCS v3.3 with me as well. 
Can I install both or do I have to uninstall v3.1 before installing v3.3?
If I have to uninstall v3.1 can I still use the flash burn 2.8, drivers and target content which came along with the board?
Thanks,
Shash
  • Hi Shash,

    a couple comments.  First of all, yes you can have both 3.1 and 3.3 installed.  Please use different directories. 

    A couple further notes.  CCSv3.3 is not officially supported in Windows 7 and also note that after installing v3.3 you will likely want to upgrade to make sure you have the latest patches and support for it.

    Please keep us informed.

    Best Regards,
    LIsa

  • Hi Lisa,

    As i mentioned in where this post originally was, http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/184028/669485.aspx#669485

     I managed to make them both work together (with windows XP).  windows 7 even failed to complete the installation without the errors all the time.

    Thanks for your valuable support. 

    Thanks,
    Shash.