This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Another kind of error from CCSv for the same very first task in connecting with the board (# 3)

Other Parts Discussed in Thread: OMAPL138

Before I posted several error msg, now new kind of error msg for the very same bug

ARM9_0: GEL: Error while executing OnTargetConnect(): Driver did not attempt to write memory at 0x01C1417C     at (*((unsigned int *) (0x01C14000+0x17C))|=((0x1<<4)&0x00000010)) [OMAPL138_1_ARM.gel:223]     at device_PLL0(0, 24, 1, 0, 1, 11, 5) [OMAPL138_1_ARM.gel:401]     at Set_Core_300MHz() [OMAPL138_1_ARM.gel:453]     at Core_300MHz_mDDR_132MHz() [OMAPL138_1_ARM.gel:247]     at OnTargetConnect() .
ARM9_0: Error: (Error -1029 @ 0x2B5F) Invalid data read from ICECrusher register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.569.0)
ARM9_0: GEL: File: G:\TI_OMAP\_MIMO_V02\OMAPL138_PRJ\spi1_comm\Debug\spi1_comm.out: Load failed.