This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS installer request

Support,

Would you please modify the installer for future CCS installations to create a Start Menu icons/folders unique to the sub-version being installed? Right now if I have v5.1.1 installed and install v5.2.0 it will over-write the v5.1.1 shortcuts. It would be ideal to be able to install multiple versions without touching existing installations in any way.

Thanks,

Tim

  • Tim,

    Although I suffer the same issue as you (I have zillions of CCS installs in my PC), the vast majority of customers have a single installation of CCS and perform updates directly to it (sometimes across version numbers), therefore creating multiple icons would create a burden for the majority of users. Keep in mind that not only the CCS icon is updated, but also Blackhawk and Spectrum Digital ones as well (if these are installed), which could quickly escalate to tens of different icons in the Desktop.

    I personally rename the CCS icons to their revisions just after a new install to avoid the issue you reported. 

    Regards,

    Rafael