This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

command line options to modify the project settings



We are making build of projects through command line scripts. The projects are created through CCS and then build and run procedure is being done by the command line.

Is there a easy way to modify the existing projects parameters like from "-02" to "-03" option or from "-ms" to none or the other way round?

We donot want to create the project from the scratch everytime but to get a flexibility to modify the project settings.

Regards

Asheesh