Other Parts Discussed in Thread: TMS320TCI6614
Hi,
I am using CodeSourcery (v 4.6.1) bare-metal (arm-none-eabi) to build an application on Windows. When I try to load the executable (simulator or device) I see that only the labels get loaded but none of the data or text. I am able to load the same executable if I use CCS v 5.0.3 correctly. I tried some applications that were built using the same version of the tool-chain and options on Linux and they seem to load correctly.
Is there some flag that need to be enabled on the windows version for CCS5.1 to work?
Regards,
Sudhanand.