CCS v 4.2.5.00005
Windows XP.
I have been using CCS 4.2.5 without issue on some C6000 based projects. I now want to do work on C5500 based projects. Apparently when I first installed CCS 4.1.2 on my machine I must have only selected the C6000 family. As a result the only two platforms or Project Types that show up (for example if creating a brand new project) are C6000 and ARM.
In comparing my ccs install to an existing install on a second PC, I see several files within PC #2 ccsv4\eclipse\plugins folder that are not in my machine. For example files like: "com.ti.ccstudio.buildDefinitions.C5500_legacy_4.1.2etc.jar. So it seems to me that I need to somehow install support for the C5500 device on my existing CCS 4.2 installation. I believe this is the core issue with another issue I posted on not being able to load an example project from the C55x CSL.
I have tried to use the "Help->software Updates->find and install" menu item, using the "Search for new features to install", selecting all Listed Sites, but nothing comes up other than C5500 code Gen tools, which I have installed but has not solved the problem.
How do I add support for the C5500 platform? Is there a specific "update Site" I should point to?
thanks
-S