Other Parts Discussed in Thread: CCSTUDIO
Hi,
I use one PC acting as build/test-server. On this PC, scripts automatically checkout sourcecode from the sourcecode repository, build it and run some tests. It seems that having the project imported into an Eclipse Workspace is required to build from command line in CCS V5.1.
The problem here is that there are checkouts to several directories in different configurations of different projects. I want to checkout a sourcecode tree (containing the CCS 5.1 projectfiles) and build one single CCS 5.1 project without caring of what is imported in the Eclipse workspace and what not on that PC. I dont even want to open CCS on this PC, it just should produce an .out file. Is this possible somehow?
bye,
Thomas