I have tried 4 times with different links. I can't get to the offline installer, I get:
Connection Interrupted
The document contains no data.
For the only on line installer I can seem to get to, here is the log end:
05/08/2012 21:12:18PM - Checking conditions for 8DC9C68D-0C93-432C-9F50-9ECCB01EE7D2 - Rename File - Before Action is Executed
05/08/2012 21:12:18PM - Checking condition 13D96D8B-3F10-4DE3-AE45-2260F3EEF34D - File Exists Condition
05/08/2012 21:12:18PM - Checking to see if <%EclipseDir%>/ccs_config.xml.bk exists
05/08/2012 21:12:18PM - ** Checking to see if C:\CCS/ccsv5/eclipse/ccs_config.xml.bk exists
05/08/2012 21:12:18PM - Condition failed
05/08/2012 21:12:18PM - Skipping action 8DC9C68D-0C93-432C-9F50-9ECCB01EE7D2 - Rename File - conditions failed
05/08/2012 21:12:18PM - Checking conditions for 05EE68FE-6C93-4340-82C2-21CF20CE1591 - Create Update.txt - Before Action is Executed
05/08/2012 21:12:18PM - Checking condition C8AE338B-8D17-4EDB-99A9-313C01CA352A - String Is Condition
05/08/2012 21:12:18PM - Checking to see if <%updates_found%> is true
05/08/2012 21:12:18PM - ** Checking to see if false is true
05/08/2012 21:12:18PM - Condition failed
05/08/2012 21:12:18PM - Skipping action 05EE68FE-6C93-4340-82C2-21CF20CE1591 - Create Update.txt - conditions failed
05/08/2012 21:12:18PM - Checking conditions for 1160585F-F26F-4111-911E-B0D10C849C31 - Remove .ij_running.txt - Before Action is Executed
05/08/2012 21:12:18PM - Checking condition 588D69A8-22C4-4BE8-A09F-5123D47D7FEF - File Exists Condition
05/08/2012 21:12:18PM - Checking to see if <%EclipseDir%>/downloads/.ijrunning.txt exists
05/08/2012 21:12:18PM - ** Checking to see if C:\CCS/ccsv5/eclipse/downloads/.ijrunning.txt exists
05/08/2012 21:12:18PM - Condition failed
05/08/2012 21:12:18PM - Skipping action 1160585F-F26F-4111-911E-B0D10C849C31 - Remove .ij_running.txt - conditions failed
~~~~~~~~~
and the output window:
Fetching org.eclipse.ui.workbench.compatibility_3.2.100.I20110413-1600.jar (2.7kB of 13.56kB at 0B/s) from http://software-dl.ti.com/dsps/dsps_public_sw/sdo_ccstudio/CCSv5/CCS5.2.0.00057_win32/eclipserepo/plugins/
An error was detected while performing the engine operation and the changes are being rolled back. See the log for details.
Preparing to commit the provisioning operation.
Committing the provisioning operation.
Installation failed.
~~~~~~~~~~~~~~~~~~
I'll try again in the morning....
Best, Dan.