Hi,
I'm trying to get the Blackhawk 560 emulator working with my 6678 EVM using CCS 5.1.1.00033. I did the install of CCS as a normal user and then driver install using the script as root. Both were successful. When I set up a target configuration file and then try the test connection button I get the following message: Cannot run program ".....a long path/ccs_base/uscif/dbgjtag.exe": java.io.IOException: error=2, No such file or directory. I'm thinking since this is Linux it should not end in .exe.
I can see the emulator when I do a lsusb but when I launch the target configuration I get an Error Initializing the Emulator: (Error -2083 @ 0x0) Unable to communicate with the emulator. Confirm emulator configuration and connections, .....
Also, if I run BH560 Conbfigu Utlity it fails to recognize the driver as well but it seems to be looking for bh560v2u.
CMD: dtc_conf get bh560v2u 0
USB: 0 devices found
Any thoughts on what to look at? I am running this on Ubuntu 12.0.4 32 bit.
Thanks,
Jack