This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

xds560 pci (TMDSEMU560PCI) memory error

hi,

   when i use XDS560 Diagnostics tool i got the following error:

********** Test XDS560 memory **********
INFO    1 XDS560 adapter boards detected
   
[adapter 0] Memory access tests on IPM
[adapter 0] Memory access tests on IDM
[adapter 0] Memory access tests on CE0
[adapter 0] Memory access tests on CE2

ERROR    [adapter 0] Memory Read does not match Memory Write on first section
        Pos: 0x00000400, Read value = 0x02303400,  Write value =    
            0x0210340

I think 0x02303400 & 0x0210340 is only "1-bit" difference.  i resoldered all 4 sdram chip but i found they are CE0 memory at last.

So ,does anyone can tell me which one on xds560 board is CE2 memory?

How can i fix this problem?

Regards,

william