Other Parts Discussed in Thread: DM3730
Hi,
I am using DM3730 SDK in Linux.
In a single C file, the main function is at the bottom of the file.
Above the main function, there are many C functions called by the main function.
In every C function, there is a printf to show which function is being called.
There is no compilation error for the ARM program.
But when I run the program in Linux prompt, the printfs show only the first few functions are being called.
What could be the problem ?
could it be the problem of stack size or heap size ?
How to change the stack size or heap size in a Linux makefile ?
Thanks,
Mr Tan