This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

specify search directories for tci files in the ccs build options does not work

Other Parts Discussed in Thread: OMAP-L137

Hi I'm working on OMAP-L137 ,in order to chang the tci file I add the new tci file to the project by just put the directiry of the tci file to the ccs build option specify search directories for tci file ,but it does not work,instead ,tci does not change ,Is there anything else I have to do ?

  • This is a Code Composer question, so it will be moved to the Code Composer Forum. Please post CCS questions there for the best chance at a good answer.

    You will need to reply back with the version of CCS you are using. You may want to restate your question and explain what you want to accomplish, because I do not understand what you are doing or why you are trying to do it.

    The extra information will help get you a helpful answer.

    Regards,
    RandyP

  • Hi,

    Randy is correct, some further details would help here about what exactly you wish to do and CCS verstion etc.   However please note that simply adding a search path does not mean CCS will attached files in that path to your project.

    Have you tried selecting your project, right-click and select "Add FIles".  Please try adding the file to your project this way and please keep us informed.  

    Best Regards,
    Lisa

  • HI,Lisa,thank you for your help.my  ccs version  is 3.3,and the platform I am using is OMAP-L137.I have this problem while i develop the dsplink between ARM and DSP.Now  i seem to solve this problem by add this line to the .tcf file manually :utiles.import File("dsplink-omapl1xxgem-base.tci");thank you!

  • HI Luo,

    ok, glad to hear you got it solved.  All the best with development.

    Best Regards,
    Lisa