Other Parts Discussed in Thread: TMS320F28027
Hello
I'm using CCSv5.1 with the TI v6.0.2 compiler and I found a bug in the compiler. I managed to isolate the problem and all that is needed to reproduce is to create a "Hello World" project with CCSv5 for TMS320F28027 and write the code below.
#include <stdint.h>
/*
* hello.c
*/
void func(uint64_t arg);
void main(void)
{
func(5);
}
void func(uint64_t arg)
{
int16_t buffer[4];
#if 1
// the following lines causes INTERNAL ERROR: no match for ASG
__byte(buffer,2) = (int)(arg >> 0);
__byte(buffer,3) = (int)(arg >> 8);
__byte(buffer,4) = (int)(arg >> 16);
__byte(buffer,5) = (int)(arg >> 24);
__byte(buffer,6) = (int)(arg >> 32);
#else
// the following works
uint32_t argHi, argLo;
argHi = (uint32_t)(arg >> 32);
argLo = (uint32_t)(arg);
__byte(buffer,2) = (int)(argLo >> 0);
__byte(buffer,3) = (int)(argLo >> 8);
__byte(buffer,4) = (int)(argLo >> 16);
__byte(buffer,5) = (int)(argLo >> 24);
__byte(buffer,6) = (int)(argHi >> 0);
#endif
}