This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSv4 update from 4.2.3 to 4.2.4 fails due to error_recovery.log (Access is denied)

Hi

A co-worker is trying to re-install CCS 4.2.3 after CCS stopped communicating with the XDS560v2. After the install, we do not have the option to create an XDS560v2 ccxml file.

So we tried to do an update to CCS 4.2.4 and got several errors in a single popup that have:

Unable to access error recover log file: "C:\Program Files\Texas Instruments\ccsv4\eclipse\configuration\org.eclipse.update\recover.log ........ (access is denied)

When we use windows explorer, the file is set to read only, but is editable if we remove the read only.

Any ideas whats happening?

Cheers