This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error using DSP

I am geeting the problem when i reset emulator of the DSP. It is showing as follows.

"Failed to reset the emulator: the error was generated by TI's USCIF driver. SC-ERR-CTL-NO-TRG-POWER<-180>. The controller has detected a target power loss. The user must turn onor connect the power supply for the target".

Please help me asap.

Thanks in advance.

 

Regards

Ramayya

  • Hi Ramayya,

    When are you resetting the emulator?

    Also, it would be helpful if you provided:

    1) What is the full version number of CCS that you are using

    2) What JTAG emulator are you using

    3) What device/board are you using

    Thanks

    ki