This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS V5.1.1 pre-configured license server - licenselocation.txt file location for install

I'm a little confused on where to place the file licenselocation.txt so it gets automatically installed by users.

The Deplyment of CCS with pre-configured license server configurations says to create a directory called license under the CCS install_image directory. I downloaded CCS v5.1.1.00031 and extracted the files. The extraction created a directory called CCS5.1.1.00031_win32 and the only directories under this are baserepo, binary, featurerepo, and features.

Is the CCS5.1.1.00031_win32 directory considered to be the install_image directory? The instructions show the following path: \install_images\ccscore\license\licenselocation.txt. I don't see a ccscore directory or install_images directory.

So my question is do I need to create this entire path or do I just create a directory called license under the directory CCS5.1.1.00031_win32?