This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can you initiate a system reset event from a GEL file?

Hi

We are currently developing an application for the C6457 and have memory protection enabled, which has proved to be very useful.  However, this has been found to cause problems when debugging via an emulator because, when launching a debug session/reloading the program data, loading of the program typically fails due to the generation of an MPC exception.  This problem could be avoided if it were possible to initiate a system reset event from the OnPreFileLoaded() callback in the GEL file, which would cause the MPC registers to be reset.  Is this possible?  We do call GEL_Reset() but this only appears to cause a CPU reset.  Clearly Code Composer can do it so it doesn't seem too unreasonable to hope that it can be done from a GEL file.

Thanks in advance

Tim