This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

code composer crash on ubuntu

Hi;

I instaled code composer on my ubuntu 10.04  PC. After installation of CCSV5.2 on Ubuntu , CCS crash at startup.

ccs_setup_5.2.0.00069.bin was locadet under /Desktop/CCS , and I instaled code composer under /usr/local/ti.

  • Hi Ibrahim,

    do you get any error logs or dump files?

    Are you running 64 bit Ubuntu?  Did you double check you have all dependent packages installed?  Did you install and launch as sudo? Did you use the full or offline installer?  Is this a fresh install?  Could you please provide a bit more information?

    Best regards,

    Lisa

  • Hi lisa . you can find dump files at the attachment. I am using a 32 bit version ubuntu kernel. I installed CCS as sudo (root@ibrahim-ubuntu:/home/ibrahim/Desktop/CCS5.2.0.00069_linux# sudo ./ccs_setup_5.2.0.00069.bin &) based on offline installer. yes it is fresh installation . I downloaded the installation file at http://processors.wiki.ti.com/index.php/Download_CCS for CCSV5.2 linux off-line version. 

  • Hi lisa . you can find dump files at the below (xpcom.txt and ds.txt. I am using a 32 bit version ubuntu kernel. I installed CCS as sudo (root@ibrahim-ubuntu:/home/ibrahim/Desktop/CCS5.2.0.00069_linux# sudo ./ccs_setup_5.2.0.00069.bin &) based on offline installer. yes it is fresh installation . I downloaded the installation file at http://processors.wiki.ti.com/index.php/Download_CCS for CCSV5.2 linux off-line version. 

    libfreebl3.so:
    linux-gate.so.1 => (0x00c30000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00f02000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00110000)
    /lib/ld-linux.so.2 (0x009ca000)
    libjavaxpcomglue.so:
    linux-gate.so.1 => (0x00ea4000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x0034d000)
    libasound.so.2 => /usr/lib/libasound.so.2 (0x00234000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00f84000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x00110000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00205000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x0072a000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00366000)
    /lib/ld-linux.so.2 (0x00761000)
    librt.so.1 => /lib/tls/i686/cmov/librt.so.1 (0x0083a000)
    libmozjs.so:
    linux-gate.so.1 => (0x0060e000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x0061a000)
    libplds4.so => /usr/lib/libplds4.so (0x009db000)
    libplc4.so => /usr/lib/libplc4.so (0x00265000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00e24000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00643000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00347000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x0036d000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x0087c000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00647000)
    /lib/ld-linux.so.2 (0x004e4000)
    libnspr4.so:
    linux-gate.so.1 => (0x00290000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00488000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00fac000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00ddb000)
    /lib/ld-linux.so.2 (0x0050e000)
    libnss3.so:
    linux-gate.so.1 => (0x00295000)
    libnssutil3.so => /usr/lib/libnssutil3.so (0x00565000)
    libplc4.so => /usr/lib/libplc4.so (0x00110000)
    libplds4.so => /usr/lib/libplds4.so (0x0075b000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00115000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00395000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00706000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x0057e000)
    /lib/ld-linux.so.2 (0x00e89000)
    libnssckbi.so:
    linux-gate.so.1 => (0x00bd1000)
    libplc4.so => /usr/lib/libplc4.so (0x00676000)
    libplds4.so => /usr/lib/libplds4.so (0x0022b000)
    libnspr4.so => /usr/lib/libnspr4.so (0x005c7000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00723000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x0077c000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x0022f000)
    /lib/ld-linux.so.2 (0x00933000)
    libnssdbm3.so:
    linux-gate.so.1 => (0x00977000)
    libnssutil3.so => /usr/lib/libnssutil3.so (0x00bdb000)
    libplc4.so => /usr/lib/libplc4.so (0x00412000)
    libplds4.so => /usr/lib/libplds4.so (0x009d0000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00dc6000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00386000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x006a8000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00227000)
    /lib/ld-linux.so.2 (0x00a30000)
    libnssutil3.so:
    linux-gate.so.1 => (0x00558000)
    libplc4.so => /usr/lib/libplc4.so (0x006c6000)
    libplds4.so => /usr/lib/libplds4.so (0x00c63000)
    libnspr4.so => /usr/lib/libnspr4.so (0x003fb000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00bc9000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00c3c000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00170000)
    /lib/ld-linux.so.2 (0x00153000)
    libplc4.so:
    linux-gate.so.1 => (0x007af000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00110000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00b4c000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x0019e000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x0031b000)
    /lib/ld-linux.so.2 (0x00a0e000)
    libplds4.so:
    linux-gate.so.1 => (0x00295000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00998000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00296000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00ca4000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x0066d000)
    /lib/ld-linux.so.2 (0x009da000)
    libsmime3.so:
    linux-gate.so.1 => (0x0094a000)
    libnss3.so => /usr/lib/libnss3.so (0x00220000)
    libnssutil3.so => /usr/lib/libnssutil3.so (0x00511000)
    libplc4.so => /usr/lib/libplc4.so (0x0076f000)
    libplds4.so => /usr/lib/libplds4.so (0x00901000)
    libnspr4.so => /usr/lib/libnspr4.so (0x0012f000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00cc1000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00d2a000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00993000)
    /lib/ld-linux.so.2 (0x00f8d000)
    libsoftokn3.so:
    linux-gate.so.1 => (0x007f8000)
    libsqlite3.so => not found
    libnssutil3.so => /usr/lib/libnssutil3.so (0x003d6000)
    libplc4.so => /usr/lib/libplc4.so (0x004ef000)
    libplds4.so => /usr/lib/libplds4.so (0x00407000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00c56000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x006e2000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x002d2000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00110000)
    /lib/ld-linux.so.2 (0x00923000)
    libsqlite3.so:
    linux-gate.so.1 => (0x00370000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00110000)
    libasound.so.2 => /usr/lib/libasound.so.2 (0x0055f000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00bbf000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x0083f000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00129000)
    /lib/ld-linux.so.2 (0x00388000)
    librt.so.1 => /lib/tls/i686/cmov/librt.so.1 (0x0071a000)
    libssl3.so:
    linux-gate.so.1 => (0x00196000)
    libnss3.so => /usr/lib/libnss3.so (0x0051d000)
    libnssutil3.so => /usr/lib/libnssutil3.so (0x00868000)
    libplc4.so => /usr/lib/libplc4.so (0x00e9c000)
    libplds4.so => /usr/lib/libplds4.so (0x00996000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00e38000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00428000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x0020f000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00213000)
    /lib/ld-linux.so.2 (0x00f49000)
    libxpcom.so:
    linux-gate.so.1 => (0x00adb000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00ae1000)
    libxul.so => not found
    libplds4.so => /usr/lib/libplds4.so (0x00b1a000)
    libplc4.so => /usr/lib/libplc4.so (0x00140000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00e64000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00159000)
    libasound.so.2 => /usr/lib/libasound.so.2 (0x0047c000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x0015d000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00bee000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x003e1000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00252000)
    /lib/ld-linux.so.2 (0x00ede000)
    librt.so.1 => /lib/tls/i686/cmov/librt.so.1 (0x00fa2000)
    libxul.so:
    linux-gate.so.1 => (0x00bb8000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00500000)
    libsqlite3.so => not found
    libmozjs.so => not found
    libsmime3.so => /usr/lib/libsmime3.so (0x00742000)
    libssl3.so => /usr/lib/libssl3.so (0x00288000)
    libnss3.so => /usr/lib/libnss3.so (0x00110000)
    libnssutil3.so => /usr/lib/libnssutil3.so (0x00224000)
    libXrender.so.1 => /usr/lib/libXrender.so.1 (0x0055c000)
    libfreetype.so.6 => /usr/lib/libfreetype.so.6 (0x00ae1000)
    libfontconfig.so.1 => /usr/lib/libfontconfig.so.1 (0x0023d000)
    libplds4.so => /usr/lib/libplds4.so (0x00bcb000)
    libplc4.so => /usr/lib/libplc4.so (0x00cd9000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00853000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00687000)
    libdbus-1.so.3 => /lib/libdbus-1.so.3 (0x007e6000)
    libX11.so.6 => /usr/lib/libX11.so.6 (0x002bb000)
    libXext.so.6 => /usr/lib/libXext.so.6 (0x0026d000)
    libpangoft2-1.0.so.0 => /usr/lib/libpangoft2-1.0.so.0 (0x00991000)
    libpango-1.0.so.0 => /usr/lib/libpango-1.0.so.0 (0x00925000)
    libgobject-2.0.so.0 => /usr/lib/libgobject-2.0.so.0 (0x007a3000)
    libgmodule-2.0.so.0 => /usr/lib/libgmodule-2.0.so.0 (0x0027d000)
    libglib-2.0.so.0 => /lib/libglib-2.0.so.0 (0x003d8000)
    libgtk-x11-2.0.so.0 => /usr/lib/libgtk-x11-2.0.so.0 (0x0bbf1000)
    libatk-1.0.so.0 => /usr/lib/libatk-1.0.so.0 (0x004a2000)
    libgdk-x11-2.0.so.0 => /usr/lib/libgdk-x11-2.0.so.0 (0x00566000)
    libgdk_pixbuf-2.0.so.0 => /usr/lib/libgdk_pixbuf-2.0.so.0 (0x004be000)
    libpangocairo-1.0.so.0 => /usr/lib/libpangocairo-1.0.so.0 (0x004d8000)
    libcairo.so.2 => /usr/lib/libcairo.so.2 (0x009da000)
    libXt.so.6 => /usr/lib/libXt.so.6 (0x005fc000)
    libgthread-2.0.so.0 => /usr/lib/libgthread-2.0.so.0 (0x00282000)
    libz.so.1 => /lib/libz.so.1 (0x004e4000)
    libasound.so.2 => /usr/lib/libasound.so.2 (0x00bcf000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00519000)
    librt.so.1 => /lib/tls/i686/cmov/librt.so.1 (0x00ad6000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x1f785000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x008d1000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x1ee04000)
    /lib/ld-linux.so.2 (0x00d30000)
    libexpat.so.1 => /lib/libexpat.so.1 (0x0064f000)
    libxcb.so.1 => /usr/lib/libxcb.so.1 (0x0053f000)
    libpcre.so.3 => /lib/libpcre.so.3 (0x0068b000)
    libXinerama.so.1 => /usr/lib/libXinerama.so.1 (0x004f9000)
    libXi.so.6 => /usr/lib/libXi.so.6 (0x00676000)
    libXrandr.so.2 => /usr/lib/libXrandr.so.2 (0x006cc000)
    libXcursor.so.1 => /usr/lib/libXcursor.so.1 (0x006bc000)
    libXcomposite.so.1 => /usr/lib/libXcomposite.so.1 (0x006c6000)
    libXdamage.so.1 => /usr/lib/libXdamage.so.1 (0x006d4000)
    libXfixes.so.3 => /usr/lib/libXfixes.so.3 (0x006d8000)
    libgio-2.0.so.0 => /usr/lib/libgio-2.0.so.0 (0x1e753000)
    libpixman-1.so.0 => /usr/lib/libpixman-1.so.0 (0x006de000)
    libdirectfb-1.2.so.0 => /usr/lib/libdirectfb-1.2.so.0 (0x00a54000)
    libfusion-1.2.so.0 => /usr/lib/libfusion-1.2.so.0 (0x00738000)
    libdirect-1.2.so.0 => /usr/lib/libdirect-1.2.so.0 (0x00768000)
    libpng12.so.0 => /lib/libpng12.so.0 (0x0077e000)
    libxcb-render-util.so.0 => /usr/lib/libxcb-render-util.so.0 (0x0081f000)
    libxcb-render.so.0 => /usr/lib/libxcb-render.so.0 (0x00824000)
    libSM.so.6 => /usr/lib/libSM.so.6 (0x0082c000)
    libICE.so.6 => /usr/lib/libICE.so.6 (0x00835000)
    libXau.so.6 => /usr/lib/libXau.so.6 (0x007e2000)
    libXdmcp.so.6 => /usr/lib/libXdmcp.so.6 (0x00888000)
    libresolv.so.2 => /lib/tls/i686/cmov/libresolv.so.2 (0x0088e000)
    libselinux.so.1 => /lib/libselinux.so.1 (0x008a2000)
    libuuid.so.1 => /lib/libuuid.so.1 (0x0084e000)

    ds.txt

    libDataSnapshotDecoder.so:
    linux-gate.so.1 => (0x00ce9000)
    libti_logger.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libti_logger.so (0x00776000)
    libXPCOMUtility.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../bin/linux_ia32/libXPCOMUtility.so (0x00c54000)
    libnspr4.so => /usr/lib/libnspr4.so (0x008e4000)
    libxpcom.so => not found
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x00d7a000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00878000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x00abf000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x009d2000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00219000)
    libxpcom.so => not found
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00110000)
    /lib/ld-linux.so.2 (0x006f8000)
    libdbusservice.so:
    linux-gate.so.1 => (0x00c2a000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00670000)
    libxpcom.so => not found
    libplds4.so => /usr/lib/libplds4.so (0x00175000)
    libplc4.so => /usr/lib/libplc4.so (0x00b50000)
    libnspr4.so => /usr/lib/libnspr4.so (0x0079d000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00992000)
    libdbus-glib-1.so.2 => /usr/lib/libdbus-glib-1.so.2 (0x00c2c000)
    libdbus-1.so.3 => /lib/libdbus-1.so.3 (0x0023e000)
    libgobject-2.0.so.0 => /usr/lib/libgobject-2.0.so.0 (0x00110000)
    libglib-2.0.so.0 => /lib/libglib-2.0.so.0 (0x00ea9000)
    libasound.so.2 => /usr/lib/libasound.so.2 (0x00277000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x00355000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x0014f000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x00179000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x0044a000)
    /lib/ld-linux.so.2 (0x00cbf000)
    libgthread-2.0.so.0 => /usr/lib/libgthread-2.0.so.0 (0x00fdf000)
    librt.so.1 => /lib/tls/i686/cmov/librt.so.1 (0x00ae2000)
    libpcre.so.3 => /lib/libpcre.so.3 (0x00907000)
    libDebugProperties.so:
    linux-gate.so.1 => (0x0062b000)
    libti_logger.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libti_logger.so (0x0070c000)
    libXPCOMUtility.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../bin/linux_ia32/libXPCOMUtility.so (0x00d79000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00754000)
    libxpcom.so => not found
    libxerces-c.so.25 => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libxerces-c.so.25 (0x00110000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x00495000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x0068c000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x00de1000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00895000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x009ee000)
    libxpcom.so => not found
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x008bd000)
    /lib/ld-linux.so.2 (0x009d1000)
    libDebugServer.so:
    linux-gate.so.1 => (0x00342000)
    libtiofr11.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../bin/linux_ia32/libtiofr11.so (0x005dd000)
    libsetup_parser.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libsetup_parser.so (0x00343000)
    libti_logger.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libti_logger.so (0x00110000)
    libXPCOMUtility.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../bin/linux_ia32/libXPCOMUtility.so (0x0013c000)
    libfsutil.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libfsutil.so (0x0016e000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x007fe000)
    libnspr4.so => /usr/lib/libnspr4.so (0x001d6000)
    libxpcom.so => not found
    libxerces-c.so.25 => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libxerces-c.so.25 (0x0fcad000)
    libjvm.so => not found
    librt.so.1 => /lib/tls/i686/cmov/librt.so.1 (0x0020b000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x00214000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00825000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x00309000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00328000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00694000)
    /lib/ld-linux.so.2 (0x008f2000)
    libxpcom.so => not found
    libimgicon.so:
    linux-gate.so.1 => (0x00907000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00dfe000)
    libgtk-x11-2.0.so.0 => /usr/lib/libgtk-x11-2.0.so.0 (0x00110000)
    libatk-1.0.so.0 => /usr/lib/libatk-1.0.so.0 (0x00861000)
    libgdk-x11-2.0.so.0 => /usr/lib/libgdk-x11-2.0.so.0 (0x00c96000)
    libgdk_pixbuf-2.0.so.0 => /usr/lib/libgdk_pixbuf-2.0.so.0 (0x004e5000)
    libpangocairo-1.0.so.0 => /usr/lib/libpangocairo-1.0.so.0 (0x007c2000)
    libpango-1.0.so.0 => /usr/lib/libpango-1.0.so.0 (0x004ff000)
    libcairo.so.2 => /usr/lib/libcairo.so.2 (0x00542000)
    libgobject-2.0.so.0 => /usr/lib/libgobject-2.0.so.0 (0x005d1000)
    libgmodule-2.0.so.0 => /usr/lib/libgmodule-2.0.so.0 (0x005bc000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00bfd000)
    libglib-2.0.so.0 => /lib/libglib-2.0.so.0 (0x00610000)
    libxpcom.so => not found
    libplds4.so => /usr/lib/libplds4.so (0x0090c000)
    libplc4.so => /usr/lib/libplc4.so (0x005c1000)
    libnspr4.so => /usr/lib/libnspr4.so (0x006da000)
    libasound.so.2 => /usr/lib/libasound.so.2 (0x00910000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00b38000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x009ee000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x00dcd000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00e17000)
    /lib/ld-linux.so.2 (0x00dad000)
    libXext.so.6 => /usr/lib/libXext.so.6 (0x00fb3000)
    libXrender.so.1 => /usr/lib/libXrender.so.1 (0x0070f000)
    libXinerama.so.1 => /usr/lib/libXinerama.so.1 (0x00719000)
    libXi.so.6 => /usr/lib/libXi.so.6 (0x0071d000)
    libXrandr.so.2 => /usr/lib/libXrandr.so.2 (0x007b2000)
    libXcursor.so.1 => /usr/lib/libXcursor.so.1 (0x007dc000)
    libX11.so.6 => /usr/lib/libX11.so.6 (0x00fc3000)
    libXcomposite.so.1 => /usr/lib/libXcomposite.so.1 (0x00898000)
    libXdamage.so.1 => /usr/lib/libXdamage.so.1 (0x00c67000)
    libXfixes.so.3 => /usr/lib/libXfixes.so.3 (0x0072b000)
    libgio-2.0.so.0 => /usr/lib/libgio-2.0.so.0 (0x00b5e000)
    libpangoft2-1.0.so.0 => /usr/lib/libpangoft2-1.0.so.0 (0x00731000)
    libfreetype.so.6 => /usr/lib/libfreetype.so.6 (0x007e6000)
    libz.so.1 => /lib/libz.so.1 (0x00758000)
    libfontconfig.so.1 => /usr/lib/libfontconfig.so.1 (0x0076d000)
    libgthread-2.0.so.0 => /usr/lib/libgthread-2.0.so.0 (0x0079d000)
    librt.so.1 => /lib/tls/i686/cmov/librt.so.1 (0x007a3000)
    libpixman-1.so.0 => /usr/lib/libpixman-1.so.0 (0x0089c000)
    libdirectfb-1.2.so.0 => /usr/lib/libdirectfb-1.2.so.0 (0x00d2c000)
    libfusion-1.2.so.0 => /usr/lib/libfusion-1.2.so.0 (0x007ce000)
    libdirect-1.2.so.0 => /usr/lib/libdirect-1.2.so.0 (0x0087d000)
    libpng12.so.0 => /lib/libpng12.so.0 (0x00ae3000)
    libxcb-render-util.so.0 => /usr/lib/libxcb-render-util.so.0 (0x007ac000)
    libxcb-render.so.0 => /usr/lib/libxcb-render.so.0 (0x007ba000)
    libxcb.so.1 => /usr/lib/libxcb.so.1 (0x00b08000)
    libpcre.so.3 => /lib/libpcre.so.3 (0x00c01000)
    libresolv.so.2 => /lib/tls/i686/cmov/libresolv.so.2 (0x00b22000)
    libselinux.so.1 => /lib/libselinux.so.1 (0x00c32000)
    libexpat.so.1 => /lib/libexpat.so.1 (0x00c6b000)
    libXau.so.6 => /usr/lib/libXau.so.6 (0x007d8000)
    libXdmcp.so.6 => /usr/lib/libXdmcp.so.6 (0x008f6000)
    libmdex.so:
    linux-gate.so.1 => (0x0093b000)
    libXPCOMUtility.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../bin/linux_ia32/libXPCOMUtility.so (0x00cab000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00706000)
    libxpcom.so => not found
    liblmgr10.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/liblmgr10.so (0x00110000)
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00e5f000)
    libti_logger.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libti_logger.so (0x00237000)
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x00416000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00263000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x00be4000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00298000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x0050b000)
    /lib/ld-linux.so.2 (0x007a4000)
    libxpcom.so => not found
    libXPCOMTILogger.so:
    linux-gate.so.1 => (0x00302000)
    libti_logger.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../../common/bin/libti_logger.so (0x0051f000)
    libXPCOMUtility.so => /opt/ti/ccsv5/ccs_base/DebugServer/linux/components/./../../bin/linux_ia32/libXPCOMUtility.so (0x00a21000)
    libnspr4.so => /usr/lib/libnspr4.so (0x00362000)
    libxpcom.so => not found
    libstdc++.so.6 => /usr/lib/libstdc++.so.6 (0x005d6000)
    libm.so.6 => /lib/tls/i686/cmov/libm.so.6 (0x00110000)
    libgcc_s.so.1 => /lib/libgcc_s.so.1 (0x00c03000)
    libpthread.so.0 => /lib/tls/i686/cmov/libpthread.so.0 (0x00c78000)
    libc.so.6 => /lib/tls/i686/cmov/libc.so.6 (0x00191000)
    libxpcom.so => not found
    libdl.so.2 => /lib/tls/i686/cmov/libdl.so.2 (0x00d18000)
    /lib/ld-linux.so.2 (0x00834000)


  • Hi Ibrahim,

    it looks like this might be a bunch of missing dependancies/packages.  So please double check that.

    http://processors.wiki.ti.com/index.php/Linux_Host_Support#Installation_Instructions

    Also please double check you have not used special or accented characters in your installation directories.  Could you please send the contents of your installjammer registry directory as well?

    Try the dependancies first and please keep us informed.

    Best Regards,

    LIsa

  • Hi Lisa , 

    Thanks for your valuable support. Yes I find some missing dependancies/packages on my host ubuntu , After reinstall those packages ccs work normally.

    thanks.

  • Hi Ibrahim,

    no problem, that is why we are here.  All the best with development.

    Best Regards,
    Lisa