Other Parts Discussed in Thread: UCD3138
Dear TI,
My question as title,
Does UCD3138 / Cyclone can compiled by version CCS4 or above??
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UCD3138
Dear TI,
My question as title,
Does UCD3138 / Cyclone can compiled by version CCS4 or above??
Ok, then I may be mistaken, as I am not that familiar with the UCD3138. Which compiler executable do you use with it in CCS 3.3?
Sorry for my question is not clear,
UCD3138 is an ARM7 base contorller for Digital Power application.
When I use CCS 3.3 compiler, I selected ARM7 device for UCD3138 to compiler C code.
It comes out a xxx.x0 file for me to load the code to controller by USB-to-GPIO connector.
I used the same way on CCS 4.0 and CCS 5.0.
But it can't not produced any xxx.x0 file.
So, I just wanna to make sure, does CCS 4.0 and CCS 5.0 support Cyclone device.
Yung-Cheng Hong said:UCD3138 is an ARM7 base contorller for Digital Power application.
When I use CCS 3.3 compiler, I selected ARM7 device for UCD3138 to compiler C code.
You can still build for ARM7 in CCSv4 and v5. When creating a new project, you can select as the Device Family as ARM, and Device Variant as Generic ARM7 Device.
Yung-Cheng Hong said:It comes out a xxx.x0 file for me to load the code to controller by USB-to-GPIO connector.
I assume the .x0 file is a hex output after converting the .out file generated by the compiler tools into hex. The default output from the TI codegen tools is .out but you probably have a step added as a post-build step in CCS 3.3 to convert the .out to .x0. If so, you can do the same in CCSv4/5, by adding a post-build step in the Project Properties->CCS Build->Build Steps tab to convert the .out file to hex.