This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RE: Beaglebone kernel debugging with CCS v5.1

HI again,

Still struggling to make run my debug "stop mode" for Jtag/USB Kernel debugging.

Now i can create a "Target configuration" file that can correctly connect and "test connection" seems OK (see below).

But when i launch my "Debug configuration" my CCS 5.1.1.00033 immediately return with the following error :



Hips .... if anyone has got an idea ?



Here are the screen-shots of my debug configuration:

1055.dbg-config-screenshots.zip



Here is my configuration file:

(Notice that i've replaced all the beginning "<" chars by a "^" as i could never preview the XML code with e2e forum HMI ?)

^?xml version="1.0" encoding="UTF-8" standalone="no"?>
^configurations XML_version="1.2" id="configurations_0">

^configuration XML_version="1.2" id="Texas Instruments XDS100v2 USB Emulator_0">
        ^instance XML_version="1.2" desc="Texas Instruments XDS100v2 USB Emulator_0" href="connections/TIXDS100v2_Connection.xml" id="Texas Instruments XDS100v2 USB Emulator_0" xml="TIXDS100v2_Connection.xml" xmlpath="connections"/>
        ^connection XML_version="1.2" id="Texas Instruments XDS100v2 USB Emulator_0">
            ^instance XML_version="1.2" href="drivers/tixds100v2icepick_d.xml" id="drivers" xml="tixds100v2icepick_d.xml" xmlpath="drivers"/>
            ^instance XML_version="1.2" href="drivers/tixds100v2cs_dap.xml" id="drivers" xml="tixds100v2cs_dap.xml" xmlpath="drivers"/>
            ^instance XML_version="1.2" href="drivers/tixds100v2cortexM.xml" id="drivers" xml="tixds100v2cortexM.xml" xmlpath="drivers"/>
            ^instance XML_version="1.2" href="drivers/tixds100v2cs_child.xml" id="drivers" xml="tixds100v2cs_child.xml" xmlpath="drivers"/>
            ^instance XML_version="1.2" href="drivers/tixds100v2cortexA.xml" id="drivers" xml="tixds100v2cortexA.xml" xmlpath="drivers"/>
            ^instance XML_version="1.2" href="drivers/tixds100v2csstm.xml" id="drivers" xml="tixds100v2csstm.xml" xmlpath="drivers"/>
            ^instance XML_version="1.2" href="drivers/tixds100v2etbcs.xml" id="drivers" xml="tixds100v2etbcs.xml" xmlpath="drivers"/>
            ^instance XML_version="1.2" href="drivers/tixds100v2pru.xml" id="drivers" xml="tixds100v2pru.xml" xmlpath="drivers"/>
            ^property Type="choicelist" Value="0" id="Emulator Selection">
                ^choice Name="Select by serial number" value="0">
                    ^property Type="stringfield" Value="ttyUSB0" id="-- Enter the serial number"/>
                ^/choice>
            ^/property>
            ^platform XML_version="1.2" id="platform_0">
                ^instance XML_version="1.2" desc="AM335x_0" href="devices/AM335x.xml" id="AM335x_0" xml="AM335x.xml" xmlpath="devices"/>
                ^device HW_revision="1" XML_version="1.2" description="AM335x" id="AM335x_0" partnum="AM335x" simulation="no">
                    ^router HW_revision="1.0" XML_version="1.2" description="ICEPick_D Router" id="IcePick_D_0" isa="ICEPICK_D">
                        ^subpath id="subpath_11">
                            ^router HW_revision="1.0" XML_version="1.2" description="CS_DAP Router" id="CS_DAP_M3" isa="CS_DAP">
                                ^subpath desc="M3_wakeupSS_0" id="M3_wakeupSS">
                                    ^cpu HW_revision="1.0" XML_version="1.2" desc="M3_wakeupSS_1" description="Cortex_M3 CPU" deviceSim="false" id="M3_wakeupSS" isa="Cortex_M3"/>
                                ^/subpath>
                            ^/router>
                        ^/subpath>
                        ^subpath id="subpath_12">
                            ^property Type="numericfield" Value="0xc" desc="Port Number_0" id="Port Number"/>
                        ^/subpath>
                    ^/router>
                ^/device>
            ^/platform>
        ^/connection>
    ^/configuration>
^/configurations>




Here is the result of the "test connection":
[Start]

Execute the command:

%ccs_base%/common/uscif/dbgjtag -f %boarddatafile% -rv -o -F inform,logfile=yes -S pathlength -S integrity

[Result]


-----[Print the board config pathname(s)]------------------------------------

/home/user/.TI/1548333067/0/0/BrdDat/testBoard.dat

-----[Print the reset-command software log-file]-----------------------------

This utility has selected a 100- or 510-class product.
This utility will load the adapter 'libjioserdesusb.so'.
The library build date was 'Feb 13 2012'.
The library build time was '22:40:23'.
The library package version is '5.0.623.0'.
The library component version is '35.34.39.0'.
The controller does not use a programmable FPGA.
The controller has a version number of '4' (0x00000004).
The controller has an insertion length of '0' (0x00000000).
This utility will attempt to reset the controller.
This utility has successfully reset the controller.

-----[Print the reset-command hardware log-file]-----------------------------

The scan-path will be reset by toggling the JTAG TRST signal.
The controller is the FTDI FT2232 with USB interface.
The link from controller to target is direct (without cable).
The software is configured for FTDI FT2232 features.
The controller cannot monitor the value on the EMU[0] pin.
The controller cannot monitor the value on the EMU[1] pin.
The controller cannot control the timing on output pins.
The controller cannot control the timing on input pins.
The scan-path link-delay has been set to exactly '0' (0x0000).

-----[The log-file for the JTAG TCLK output generated from the PLL]----------

There is no hardware for programming the JTAG TCLK frequency.

-----[Measure the source and frequency of the final JTAG TCLKR input]--------

There is no hardware for measuring the JTAG TCLK frequency.

-----[Perform the standard path-length test on the JTAG IR and DR]-----------

This path-length test uses blocks of 512 32-bit words.

The test for the JTAG IR instruction path-length succeeded.
The JTAG IR instruction path-length is 6 bits.

The test for the JTAG DR bypass path-length succeeded.
The JTAG DR bypass path-length is 1 bits.

-----[Perform the Integrity scan-test on the JTAG IR]------------------------

This test will use blocks of 512 32-bit words.
This test will be applied just once.

Do a test using 0xFFFFFFFF.
Scan tests: 1, skipped: 0, failed: 0
Do a test using 0x00000000.
Scan tests: 2, skipped: 0, failed: 0
Do a test using 0xFE03E0E2.
Scan tests: 3, skipped: 0, failed: 0
Do a test using 0x01FC1F1D.
Scan tests: 4, skipped: 0, failed: 0
Do a test using 0x5533CCAA.
Scan tests: 5, skipped: 0, failed: 0
Do a test using 0xAACC3355.
Scan tests: 6, skipped: 0, failed: 0
All of the values were scanned correctly.

The JTAG IR Integrity scan-test has succeeded.

-----[Perform the Integrity scan-test on the JTAG DR]------------------------

  • Emilie,

    I split the thread as it seems this issue has an unrelated root cause.

    Usually these java.lang.NullPointerException errors are caused by a missing install file (one of the DebugServer files) or simply a somewhat corrupt workspace/configuration files.

    For the first scenario a reinstall would be the best solution, but before you do that please follow the steps shown in the sections General IDE and Debugger of the CCS Troubleshooting page below:

    http://processors.wiki.ti.com/index.php/Troubleshooting_CCS

    Hope this helps,

    Rafael