I am using old CCS v3.3. The project I am working on is written on C++ for 5505 DSP.
Each time I reset cpu via menu Debug -> Reset CPU the assembler window pops up.
The same happens if I connect to DSP via Debug -> Connect or load program to DSP via
File -> Load Program menu.
Can anyone explain how can I prevent poping up these annoying assembler windows?
Thanks