This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Failed to initialize the Debug Server: Cannot read system setup data from XML file <Path>



I am getting the following error when I try to Debug a project that was built on a different computer in a different directory. (See Image)

"Exception occurred during launch

Reason:

Failed to initialize the Debug Server

Reason: Cannot read system setup data from XML file <Path>.ccxml

Error parsing file:

..."

If copy the .ccxml file to the directory that is listed the error goes away, but I haven't been able to find a way to tell Code Composer that the file already exist in the location from which I opened the project. Is there a setting somewhere or some other way to get CC to look in my working directory for this file and not the absolute path of where this project was originally created on a different computer? I really don't want to have to recreate the entire directory structure for every imported project.

Thanks for the help

 

 

  • Hi Darnell,

    have you tried adding the ccxml to the project by drag and drop or right click and select "add files"?

    When you install CCS there is "default" ccxml directory (if you create a new target configuration you will see this directory and see there is an option to use it).  This should be on your own PC and available to all projects/workspaces.  Have you looked at that?

    Please keep us informed.

    Best Regards,

    Lisa

  • Hi Darnell,

    just wanted to see whether there is any update to your enquiry here ..?

    Best Regards,
    Lisa