This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using doxygen and eclox in Code Composer Studio v.4.2.3

Hi,

I use Code Composer Studio v4.2.3. I want to use doxygen inside CCS. Therefore I installed eclox, which is an doxygen frontend for eclipse. CCS is eclipse based. Thus, I thought that should work. In eclipse it works, but not in CCS. When I try to open the doxygen file I can´t and get the error message:

"Unable to create this part due to an internal error. Reason for the failure: The editor class could not be instantiated. This usually indicates that the editor's class name was mistyped in plugin.xml."

For that I have two questions:

1) Does anybody use doxygen with CCS v4.2.3 - is it possible?

2) Are there other code documentation tools for CCS, which work similar to doxygen?

regards,

Gerd