This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

data transfer from DSK to PC

Hi all.

I have DSK C6713, and I want to transfer data from DSK to PC.

Does use RTDX in KIT to do that?

How to use that? 

I have matlab vesion 6.5 and CCS 3.1, and I process them, but It do not run.

Here my project: http://dl.dropbox.com/u/59575236/rtdx_matlab_sim.rar

I think my version of Matlab and CCS do not support for this.

Please help me.

Thanks.

Regards! Linh

  • Hello Linh,

    CCS 3.1 does support RTDX. I'm not sure for certain if Matlab 6.5 is compatible with CCSv3.1 but I believe so. You can confirm this with Mathworks. If you are not getting any communication between CCS and Matlab via RTDX, then check to make sure you have enabled RTDX in CCS and also try some of the RTDX diagnostics tests in CCS.

    'Tools -> RTDX -> Configuration Control' to enable it. Once enabled, run the tests via:

    'Tools -> RTDX -> Diagnostics Control'. if the tests pass, then it is working from a CCS standpoint.

    Hope this helps

    ki