HI, I am not able to complete ccs5.2 install because of following problem. I was upgrading from ccs5.1 to ccs 5.2, and the install folder chosen is different from that of CCS5.1.
This occurred when CCS was auto discovering the extension sites.
Operation details
Cannot complete the install because one or more required items could not be found.
Software being installed: RTSC/XDCtools (IDE Client) 3.23.1.43 (org.eclipse.rtsc.xdctools.product.ui.feature.group 3.23.1.43)
Missing requirement: XDC RTA Plug-in 3.23.1.43 (com.ti.rta 3.23.1.43) requires 'bundle com.ti.dvt.rta.interfaces 0.0.0' but it could not be found
Cannot satisfy dependency:
From: RTSC/XDCtools (IDE Client) 3.23.1.43 (org.eclipse.rtsc.xdctools.product.ui.feature.group 3.23.1.43)
To: com.ti.rta [3.23.1.43]
Regards,
Pankaj