Other Parts Discussed in Thread: TMS320C6455
I need to load and run a .out file on a TMS320C6455 board using a Blackhawk USB-560m emulator. In CCS v3.3 I was able to do this very simply through the following steps: Debug->Connect, Debug-> Reset, File->Load Program, and Debug->Run. It was not required to open a project. Is there an equivalent way to do this with CCS v5? The interface is very different from V3.3 and I can't find these commands in the menus.
Thanks,
Dan