Other Parts Discussed in Thread: OMAPL138
If you use BeagleBone, OMAPL138 or OMAP4430 or OMAP4460 devices, this note is for you:
o Compatibility break: a target configuration file (.ccxml) created with one of the production versions of CCSv5 that uses OMAPL138, OMAP4430 or OMAP4460 will fail to be launched by the debugger. To repair this, simply double-click the target configuration file (.ccxml) inside CCS, select the tab “Basic” and simply uncheck and re-check the device selected. The reason for the break is the addition of certain auxiliary cores (PRU to OMAPL; PTM to OMAP4).
o If a target configuration file (.ccxml) for the BeagleBone was created using CCSv5.2 Beta 3, it will need to be repaired by following the method above.