This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I'm trying to build a few projects from the command-line using eclipsec. Here is the call:
C:\ti\ccsv5\eclipse\eclipsec -noSplash -data "../temp_boot" -application org.eclipse.cdt.managedbuilder.core.headlessbuild -importAll "../Bootloader_I2C_EEPROM" -cleanBuild "Bootloader_I2C_EEPROM/Debug" -build "Bootloader_I2C_EEPROM/Debug" > BootBuild.txt >&2
It fails with the libc.a compatible library issue when I try the boot project I have because it doesn't find any source files (they are virtual). The larger projects have a mix, since a few are thrown in the project folder and brought in automatically by Eclipse and everything else is a virtual folder/file. My command-line build scripts for those fail with linker errors because it doesn't include the virtual files in the build.
Is there a fix for this?
(I don't have program mode compilation turned on, as another poster found fixes his/her problem).
Thanks
Operating Environment
CCS v.5.1
Windows 7
C6457
Scripting Language: Dos Batch file
Hi William,
We see that you are using the standard CDT headless build command. Could you try using the CCS headless build commands?
http://processors.wiki.ti.com/index.php/Projects_-_Command_Line_Build/Create
Also could you explain what you mean by your files being virtual? Do you mean they are linked source files?
Thanks
ki