I bought a floating license for CCS 5.1
I’ve installed the Flexnet license server on my computer and imported the license file I received from TI.
Now when I run the CCS on the same computer on which the license server is running everything works as expected: The CCS reports it is Licensed and in the FlexNet License Administrator Dashboard I see that one CCS_DEBUGGER license is in use.
The problem is that I can’t get it to work with CCS 5 that is installed on another computer.
I configured the License Server Manager to use port 27000, and the Vendor deamon(tidspssw) to work on port 27001.
In the CCS on the computer I configured the License server to connect to port 27000 on the computer where the license server is running.
When I run a network monitor and open CCS on the remote computer I see that the remote computer connects to the license server manager on port 27000 and the connects to tidspssw.exe on port 27001,
So I’m pretty sure that the problem is NOT with the communication…
I’d appreciate it if somebody could help me with this problem..
Thanks,
Nadav