This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 with XDS100v2

Hi,

We have DM368 based custom hardware.

Flashing UBL and UBOOT using the NAND_WRITER program is proving difficult.

Code Composer (5.2 Linux) takes quite a long time to run it's startup sequence once connceted to the board and then I load the program Nand_writer.

However, the problem really starts after the program is loaded - I click on "Resume" and most times, the board appears to simply reset and the program does not get executed.

It's obviously possible that this could be a problem with the board but if anyone has any expereience of this issue with a similar set-up I'd like to know if you managed to solve it!

Regards,

Will.