The documentation tells me that I will find the On-Chip Flash Programmer in the Code Composer 5 Debug perspective under the Tools tab. I do not. Should I? Is the documentation wrong?
I have followed instructions found in a post (with the same subject line as the one I'm using for this POST) on how to find the SDFlash.exe file which I assume can be used as a standalone tool. But this answer did not address the original question about finding the On-Chip Flash Programmer under the Tools tab. Is it supposed to be there? Is the SDFlash.exe tool the same thing or is it a substitute for a deleted tool?
I just want to clarify. The documentation tells me one thing, the E2E posting tells me another. I want to believe.