I have a problem with the debug session of the am335x, after I have updated ccs. If I load a programm on the chip it is loaded and starts running immediatly. In ccs 5.1 I had to click the "run" button. The biggest problem I have that the code is not executed. Are there any suggestions how I can solve this or must I unisntall ccs 5.2 ?