While trying to build an example on the CCSv5 I encountered a problem:
I tried to make a c6000 CCS project. Using the example for the DSP/BIOS 5.xx Examples on the evmOMAPL137 Examples list:
I tried the clk Example. and it comes with 2 files: clk.c and clk.tcf
The thing is when I compile, it doesn't generate the .cmd file and the clkcfg.h file. I don't understand what's going on, probably I've messed up with some configuration but this is a fresh install of the 5.2 version of the Code Composer. I would like an answer on this topic as I didn't have this problem with the first release of the CCSv5.
Regards,
Aquiles Lacruz