Hi,
I download CCS 5.2 Windows free evaluation and it works well. From the on line tutorial videos, I realize that the new SYS/BIOS has many new features. I only see DSP/BIOS when I select "File/New/DSP/BIOSv5.x configuration File". I see the folder structure is:
.................................
C:\ti\bios_5_41_11_38
C:\ti\bios_6_33_03_34
C:\ti\bios_6_33_05_46
ccsv5
grace_1_10_03_30
ipc_1_24_02_27
uia_1_00_03_25
xdais_7_21_01_43
xdais_7_21_03_53
..........................
When I right click a project, then "Property", it shows at the bottom:
DSP/BIOS support
DSP/BIOS version: 5.41.11.38
I click "More" button at the right side. It shows present setting: "Select tool version: 5.41.11.38". There is no other bios version in the pull down bar.
Then, I press radio button "Select tool from file-ssytem:" Even I select the folder: "C:\ti\bios_6_33_05_46", press "OK", the DSP/BIOS version is still 5.41.11.38. What is wrong with my system? How can I get version 6 DSP/BIOS?
Is my problem related to XDCtools installation?
I just check a project property. It is not shown as a thread metioned:
Project->Properties->CCS Build->XDCtools->Advanced Options
My project property is:
Project->Properties->Build
There is no CCS Build. There is no XDCtools. But I have installed XDCtools before. There is XDCtools folder: C:\ti|xdctools_3_23_03_53. As I click: Start\All Programs\XDCtools 3.23.03.53, there are several XDC applications. One is XDC Repository Manager. What is wrong with my system?
Thanks