Other Parts Discussed in Thread: CCSTUDIO
Hello,
I am new to CCS and TI processors. I am using CCS 3.1.0 on Windows XP Professional with the C6416 DSK and wanted to run the examples delivered together with the IQ-math library. The library is installed in 'C:\iqmath\'. After opening a project file, e.g. 'fir_IQ.pjt' and building the project, I get the following error message:
[FIRComplex_float.c] "C:\CCStudio_v3.1\C6000\cgtools\bin\cl6x" -g -k -fr"C:/iqmath/example/FIR/Debug" -fs"C:/iqmath/example/FIR/Debug" -ft"C:/iqmath/example/FIR/Debug" -fb"C:/iqmath/example/FIR/Debug" -i"../../include/" -i"../../../include/" -i"../bmrksrc" -d"MATH_TYPE=IQ_MATH" -d"DEBUG" -d"GLOBAL_Q=27" -mw -mh -mi -mv6400+ -@"../Debug.lkf" "FIRComplex_float.c"
>> ERROR: cannot run cmp6x - file could not be found
which is the same for all .c files in the project as well as for the other example projects. The path to the cgtools is correct.
The linker is set in the build options as follows: -c -m".\Debug\fir_IQ.map" -o".\Debug\fir_IQ.out" -w -x
Do I need to set any additional search paths to build the project correctly?
Thank you very much,
Matthias