This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem with linking rts64plus_elf_eh.lib

my greeting

I am trying to build (http://cppunit.sourceforge.net/doc/lastest/money_example.html) in CCS 5.1

and problem appaers during linking phase :

**** Build of configuration Debug for project Money ****

H:\ti\ccsv5\utils\bin\gmake -k all

'Building file: ../Source/MoneyApp.cpp'

'Invoking: C6000 Compiler'

"H:/ti/ccsv5/tools/compiler/c6000/bin/cl6x" -mv64+ -g --exceptions --rtti --include_path="H:/ti/ccsv5/tools/compiler/c6000/include" --include_path="H:/workspace_v5_1/Money/include" --display_error_number --diag_warning=225 --abi=eabi --preproc_with_compile --preproc_dependency="Source/MoneyApp.pp" --obj_directory="Source" "../Source/MoneyApp.cpp"

'Finished building: ../Source/MoneyApp.cpp'

' '

'Building file: ../Source/MoneyTest.cpp'

'Invoking: C6000 Compiler'

"H:/ti/ccsv5/tools/compiler/c6000/bin/cl6x" -mv64+ -g --exceptions --rtti --include_path="H:/ti/ccsv5/tools/compiler/c6000/include" --include_path="H:/workspace_v5_1/Money/include" --display_error_number --diag_warning=225 --abi=eabi --preproc_with_compile --preproc_dependency="Source/MoneyTest.pp" --obj_directory="Source" "../Source/MoneyTest.cpp"

'Finished building: ../Source/MoneyTest.cpp'

' '

'Building file: ../Source/StdAfx.cpp'

'Invoking: C6000 Compiler'

"H:/ti/ccsv5/tools/compiler/c6000/bin/cl6x" -mv64+ -g --exceptions --rtti --include_path="H:/ti/ccsv5/tools/compiler/c6000/include" --include_path="H:/workspace_v5_1/Money/include" --display_error_number --diag_warning=225 --abi=eabi --preproc_with_compile --preproc_dependency="Source/StdAfx.pp" --obj_directory="Source" "../Source/StdAfx.cpp"

'Finished building: ../Source/StdAfx.cpp'

' '

'Building target: Money.out'

'Invoking: C6000 Linker'

"H:/ti/ccsv5/tools/compiler/c6000/bin/cl6x" -mv64+ -g --exceptions --rtti --display_error_number --diag_warning=225 --abi=eabi -z -m"Money.map" --stack_size=0x2000 --heap_size=0x2000 --warn_sections -i"H:/ti/ccsv5/tools/compiler/c6000/lib" -i"H:/ti/ccsv5/tools/compiler/c6000/include" --reread_libs --rom_model -o "Money.out" "./Source/StdAfx.obj" "./Source/MoneyTest.obj" "./Source/MoneyApp.obj" -l"rts64plus_elf_eh.lib" "../Source/CPPUnitLib.lib"

<Linking>

warning: automatic library build: using library

"H:/ti/ccsv5/tools/compiler/c6000/lib/rts64plus_elf_eh.lib" for the first

time, so it must be built. This may take a few minutes.

'[' is not recognized as an internal or external command,

operable program or batch file.

'[' is not recognized as an internal or external command,

operable program or batch file.

'cl6x' is not recognized as an internal or external command,

operable program or batch file.

gmake.exe[1]: *** [c:/docume~1/mijova~1/locals~1/temp/tid860~1/obj/decode.obj] Error 1

'cl6x' is not recognized as an internal or external command,

operable program or batch file.

gmake.exe[1]: *** [c:/docume~1/mijova~1/locals~1/temp/tid860~1/obj/negll.obj] Error 1

'cl6x' is not recognized as an internal or external command,

operable program or batch file.

gmake.exe[1]: *** [c:/docume~1/mijova~1/locals~1/temp/tid860~1/obj/wchar.obj] Error 1

'cl6x' is not recognized as an internal or external command,

operable program or batch file.

This librarys is part of CCS 5.1

Thank you in advance