Other Parts Discussed in Thread: CCSTUDIO
Hi
I'm trying to build projects meant for CCSv2 by using CCSv5 (using CCSv2 CG tools) due to some compatibility issues concerning Windows7.
I have exported a project makefile using CCSv2 so far, but right now, I'm not able to create a new CCSv5 project in which I could build this project.
I tried this command:
eclipsec –noSplash -data "C:\Workspace" -application com.ti.ccstudio.apps.projectCreate -ccs.name test_project -ccs.device com.ti.ccstudio.deviceModel.C5500.GenericC55xxDevice -ccs.autoGenerateMakefiles false -ccs.makefileName "Portatil.mak"
that generated a "Standard Make project". Then I used the 'Project -> Import existing CCS Eclipse Project' to open it and imported the project files into it (and copied the makefile in its ROOT).
After that, if I hit the 'Build' button I get the next error message:
C:\ti\ccsv5\utils\bin\gmake -k all
Cannot run program "C:\ti\ccsv5\utils\bin\gmake": El nombre del directorio no es válido. (File name not valid)
Error: Program "C:/ti/ccsv5/utils/bin/gmake" is not found in PATH
Can anybody tell me what am I doing wrong?
I will appreciate every help.
Gonzalo