I use the TMDSHVMTRPFCKIT F28035 control card
Error connecting to the target:
(Error -1 @ 0x1452)
This '-1' value should be returned only during code development.
It is a temporary value used when a more appropriate error value
has not yet been assigned. This is the most negative of the three trivial
error numbers that are used by USCIF adapters, drivers and utilities.
(Release 5.0.333.0)
C28xx: Failed Software Reset: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Release 5.0.333.0)
C28xx: Trouble Reading PC Register: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Release 5.0.333.0)
C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Release 5.0.333.0)
C28xx: GEL: Error while executing OnReset(1): Target failed to read the register ST1.
C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Release 5.0.333.0)