Is ıt possible to use ccs v3.3 and xds100v1 on win7x64 ? I couldn't see xds100 emulator on CCS SETUP after install, also service pack 12 and xds100 drivers giving error, is it because of 64 bit system?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is ıt possible to use ccs v3.3 and xds100v1 on win7x64 ? I couldn't see xds100 emulator on CCS SETUP after install, also service pack 12 and xds100 drivers giving error, is it because of 64 bit system?
Hi,
are you having general CCS issues? CCSv3 is not officially supported on Win 7 however has been know to function. You may need to check a compatibility mode etc.#
The first XDS100 driver release that supported 64bit was in CCSv4.0.2. I don't believe the software package for CCSv3.3 supports 64bit.
I have been able to use XDS100 with Win7 64bit fine.
Best Regards,
Lisa
Hi,
Thanks for the answer. Yes I had problems installing XDS100v1 with CCS v3.3 on win7x64 . I was able to install ccs but couldn't make it recognize xds100. Now I'm going to try it on winXP. I thought that using a 32bit older system for a old version of ccs can be better.