Other Parts Discussed in Thread: OMAP3530, CCSTUDIO
I am using syslink_2_10_6_28 and Linux Kernel V3.0.28. I have two projects in CCSV5.2, one is the Linux Kernel project and the other is Syslink project. I can set a breakpoint in module.c to find the load address for syslink.ko, but I do not see a way to load the symbols for syslink.ko and how to relate the kernel module to the Syslink project source files. This load address matches output of 'cat /proc/modules'. I have also reviewed several posts in this forum regarding kernel module debugging, but they reference Linux Aware debugging from CCSV4 and since I understand that there is no Linux Aware debugging in CCSV5.2, nothing seems to be working for me.
Regards,
John