This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

similar problem

Other Parts Discussed in Thread: CCSTUDIO, TMS320C6474

Hi Jhon

i have similar problem

i am working on the CCS V3.3 with evm320C6474 for more than 2 years now but for some reason which i don't know it started to crash each time i start it,so i tried to reinstall it,and the message box: "Unable to find an appropriate registry key for "ICEPick_C" start to pop up .

i tried every suggestion in this forum and the message changed to "Unable to load C:\CCStudio_v3.3\drivers\sdgoicepick_bypass.dvr" i checked the registry "HKEY_LOCAL_MACHINE\SOFTWARE\Texas Instruments\CCS_\ICEPick_C\Tpi\Reserved" and it not foud there is only under Default and Fileame.

I hope you can help me

Best regards

Mechael

  • Hello Mechael,

    i suspect that the working CCSv3.3 you had had been patched with some update patch. Did you install the same patch with your new install? Also sounds like you are using Spectrum Digital emulators. Did you install their drivers? It doesn't come with 3.3 by default.

    Thanks

    ki

  • Hi ki

    i don't remember that i patch some thing with  CCS i may upgraded the bios version only.

    i am using the TMS320C6474 this board contain a build in emulator (in the board) and the driver is already installed in (i can see it in the device manager ).

    the cd added to the box of the TMS320C6474  contain the CCS V3.3 and the driver for that specific card .

    thanks

  • Ok so you have CCSv3 kit version which is tied to the kit only and cannot be upgraded.

    It could be that your registry got corrupted. You may need to fully uninstall CCSv3 and then reinstall it.