Hi all,
I use CCS V5 with a floating license. Now I need the CCS V5 on a laptop without a continuouse connection to the license server. Can I do that?
In the documentation of the FlexNet server I found the "Mobile Licensing" Feature. Is the CCS licens ready for mobile licensing?
Mobile Licensing
End users often want to use applications on computers that do not have a continuous connection to a license
server. These situations include:
• Working on a laptop
• Using a computer both at work and at home
• Working from several different computers not connected to a license server
FlexNet Publisher supports licenses that allow one of several kinds of mobile licensing:
• Node-locked to a laptop
• Node-locked to a FlexNet ID dongle
• Node-locked to a FlexNet ID dongle with FLOAT_OK keyword
• License borrowing with BORROW keyword
• Node-locked to a user name
• Fulfilled from a prepaid license pool
• Optionally when provided by the publisher, Distribution of Node-Locked Licenses to Networked Machines
using trusted storage can be used.
You should use license rehosting if an enterprise wants to move a license without using one of these methods. Th
software publisher must generate a new node-locked license file for each new client computer. Rehosting require
administrative overhead because the software publisher must be involved with each move.
thanks Jens