Good morning,
I wondered if anyone could please help me with the following issue, when pressing the "Test Connection" button on the new target configuration screen I get the following output:
[Start]
Execute the command:
%ccs_base%/common/uscif/dbgjtag.exe -f %boarddatafile% -rv -F inform,logfile=yes -S pathlength -S integrity
[Result]
The [-d/-f] or [-X] options were not used.
This utility requires an emulator program or adapter file.
The board configuration file either did not name it at all,
or the named file was not found or lacked read permission.
The features of this utility are explained in the
[-h] option's brief help and the documentation.
[End]
I've tried searching the forum to no avail. Anyone got any leads?
Thanks a lot,
Mark