Hello,
I recently installed CCSv5.2 on my System and converted a CCS v4.2.4.33 project with no issues, however I cannot get the BH-USB-560M Emulator to function, invariably CCS v5.2 hangs as soon as code dowload to the target device starts (USB LED goes red on the Emulator).
Some context information:
- Both CCS v4.2 and CCS v5.2 are installed on my Win7 x64 Bit PC.
- CCS v5.2 was installed on my System with CCS v4.2 already installed, to a different location.
- Both binaries compiled form the same sources and linked by CCS v4.2 and CCS v5.2 function correctly on the Target DM6446 based platform.
- I can switch back to CCS v4.2 and the Emulator functions perfectly and can start a Debug session.
- Note that the CCS v5.2 did install newer drivers for the Blackhawk emulator and they seem to work in CCS v4.2 also.
- In CCS v5.2 the Target Configuration parameters are identical to the settings in CCS v4.2.
- "Test Connection" in CCS v5.2 Target Configuration reports no errors.