This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Specify the file build options with the command line.

Expert 7680 points

Hi Champions,

I use the command line to create and build the project with the CCSv5, and I have the request that different files/folders use different optimization level,  the option -ccs.setCompilerOptions only set the project build options, any idea to implement it. Thank you.

Zhan.