Everytime I try to uninstall the software on XP SP3 using the Add/Remove control panel, all it does is repair the installation. Are there manual install instructions or a dedicated uninstaller somwhere?
This is a bit urgent to work out. Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Everytime I try to uninstall the software on XP SP3 using the Add/Remove control panel, all it does is repair the installation. Are there manual install instructions or a dedicated uninstaller somwhere?
This is a bit urgent to work out. Thanks!
Hi Joshua,
what software are you installing/uninstalling? CCS? The MSP drivers should normally be well manged by CCS itself although there is the v2 and v3 dlls for which there is an upgrade/downgrade utility. Have you seen this wiki? Can you explain exactly what you are doing?
http://processors.wiki.ti.com/index.php/MSP_Debug_Stack
Best Regards,
Lisa
This was an interesting situation that I resolved by doing a complete uninstall of CCS, both 5.1 and 5.2. I think that there was some version incompatibility between the drivers? I am honestly not sure, but after reinstalling 5.1 I am able to program. Unfortunately, I do not have any time to debug this further at this point.
Likely the problem is related to the upgrade/downgrade issues as mentioned in the wiki. Either way, it is working.
I would like to know whether or not there are dedicated, non-forum support for paid CCS licenses to actually call to resolve issues? In a production environment while the forums are nice, some problems do need to be resolved quicker.
Thanks.
Hi Joshua,
glad to hear you are up and running.
Regarding your support question. If you have an FAE/local agent this is then the best first point of contact for you. Otherwise for technical matters, we find this the best solution.
All the best with development.
Best Regards,
Lisa