This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error: Import failed for project 'xxx' because its meta-data cannot be interpreted. Please contact support.

I get one of these errors for every project I try to import.  I am using CCSv5.1.  Going to v5.2 is out of the question because the project imports are 10 times as long.

I think that the problem is related to requests to make .project files writable when the workspace is created.  These files are under version control and should not need to be checked out if you are just going to make a build.  How can a build be repeatable if the files making the build get re-written every time?

Any ideas?