Other Parts Discussed in Thread: SYSBIOS, CCSTUDIO
Hi,
I ran into the problem, that CCS crashes completely when I try to enter a symbol name in the Memory Browser or in the field 'start address' of the graph tool (single time for example). When I use the address of according array both 'tools' are working fine. I figured out, that it doesn't matter if the symbol name actually exists or not. CCS crashes anyway.
The following screen shot shows the way I usually use the Memory Browser with symbol names.
System Environment:
Ubuntu 12.04 LTS (32 Bit)
CCS 5.1.1.00033
XDS560v2 STM
Target: SoC with C674x
Please find attached the CCS_workspace/.metadata/.log, the CCS install log and the java dump file.
EDIT: System Environment