I currently have a project that uses linked source files. I have configured the project to use CVS from within ccs5 and can commit the project to CVS. My problem is that I cannot commit the linked folder/files with the project. If I look at the properties for the linked folder and go to CVS it says "This folder is ignored by CVS." Is there a way I can get ccs5 to include these folder/files when I commit?